cancel
Showing results for 
Search instead for 
Did you mean: 

Additional Node support

Michael Dalby
Associate II

Hello, I wondered if you will add the ability to import/add new nodes to the STM32CubeMonitor system from the Node Red Library (https://flows.nodered.org/)?

After all this is one of the strengths of the Node Red system to enable the use of collabrative built nodes.

Many thanks

Michael

1 ACCEPTED SOLUTION

Accepted Solutions
stephane.legargeant
ST Employee

Hello Michael

It is possible to add nodes in the palette with the menu "Manage Palette".

0693W000000VDdhQAG.png

You may not see the menu because Node-Red uses npm to install nodes, and the menu "Manage Palette" is not available when npm is not installed on the computer.

In order to add nodes in the palette, you need to install nodejs (with npm). Then the menu will be available, you will have access to Node-RED nodes.

Best regards

Stephane

View solution in original post

2 REPLIES 2
stephane.legargeant
ST Employee

Hello Michael

It is possible to add nodes in the palette with the menu "Manage Palette".

0693W000000VDdhQAG.png

You may not see the menu because Node-Red uses npm to install nodes, and the menu "Manage Palette" is not available when npm is not installed on the computer.

In order to add nodes in the palette, you need to install nodejs (with npm). Then the menu will be available, you will have access to Node-RED nodes.

Best regards

Stephane

Michael Dalby
Associate II

Hi Stephane

Thats excellent news.... many thanks

Michael