2020-03-26 7:22 AM
In STM32CubeIDE it seems that index don´t work. I tried refresh it, but it didn´t help.
This happens when I import existing project into workspace. We tried it on multiple projects and multiple computers, but so far nothing has solved this problem
2020-03-27 1:46 AM
Hello @Pavel Širů�?ek
Could you please tell me which STMCubeIDE version did you use.
Please tell me more about the scenario to check the issue.
Best regards,
Nesrine
2020-03-27 2:13 AM
Hello,
thank you for quick response.
I use Version: 1.2.1
Build: 5190_20200115_1224 (UTC)
When i CTRL + left mouse click a function name, this should switch me to function definition (or define, variable, etc...). This works for functions automatically generated from CubeMX. (For example function HAL_GPIO_WritePin works as expected.) But it doesn't work for functions written by myself. IDE throws a error Could not find symbol "function_name" in index. In Attolic, this was working well.
Best regards,
Pavel
2020-03-27 3:05 AM
Hi @Pavel Širů�?ek
Thanks for your feedback, the reported problem will be reviewed by STM32CubeIDE development team.
Best regards,
Nesrine
2020-04-02 6:04 AM
Hello @Pavel Širů�?ek
Are your files physically inside the project or linked in from external drive?
Have you tried right-clicking on the project and Indexer --> Re-build?
Index can go broken if you modify/add files outside Eclipse awareness, for example with another external editor...
Regards,
Nesrine
2020-04-02 6:10 AM
or Networked / Shared drive?
2020-04-02 8:40 AM
Hello,
Files are on the same drive but in different location than folder with .project.
Yes, i tried re-build the indexer.
Im adding files by simply copy+pasting them to folders. Is this the problem?
Thank you,
Pavel
2020-04-07 6:16 AM
Hello @Pavel Širů�?ek
Could you please provide us the structure (in text form is fine, for example C:/MyProjects/MyProject) for the project and for the additional files creates that experiences the error when CTRL + clicking them? Also a screenshot of the Project Explorer view might be helpful.
Best regards,
Nesrine
2020-04-17 7:43 AM
Hello,
sure. Project location is:
D:/fw/projects/projectName/.project
And sources location is:
D:/fw/sources/common/example1.h
D:/fw/sources/common/example1.c
D:/fw/sources/drivers/adc_driver.h
D:/fw/sources/drivers/adc_driver.c
Workspace location is:
D:/fw/workspaces/projectName/
Project setting:
<?xml version="1.0" encoding="UTF-8"?>
<projectDescription>
<name>projectName</name>
<comment></comment>
<projects>
<project>RemoteSystemsTempFiles</project>
</projects>
<buildSpec>
<buildCommand>
<name>org.eclipse.cdt.managedbuilder.core.genmakebuilder</name>
<triggers>clean,full,incremental,</triggers>
<arguments>
</arguments>
</buildCommand>
<buildCommand>
<name>org.eclipse.cdt.managedbuilder.core.ScannerConfigBuilder</name>
<triggers>full,incremental,</triggers>
<arguments>
</arguments>
</buildCommand>
</buildSpec>
<natures>
<nature>org.eclipse.cdt.core.cnature</nature>
<nature>org.eclipse.cdt.managedbuilder.core.managedBuildNature</nature>
<nature>org.eclipse.cdt.managedbuilder.core.ScannerConfigNature</nature>
<nature>com.st.stm32cube.ide.mcu.MCUProjectNature</nature>
<nature>com.st.stm32cube.ide.mcu.MCUCubeIdeServicesRevAProjectNature</nature>
<nature>com.st.stm32cube.ide.mcu.MCUManagedMakefileProjectNature</nature>
<nature>com.st.stm32cube.ide.mcu.MCUEndUserDisabledTrustZoneProjectNature</nature>
<nature>com.st.stm32cube.ide.mcu.MCUSingleCpuProjectNature</nature>
<nature>com.st.stm32cube.ide.mcu.MCURootProjectNature</nature>
</natures>
<linkedResources>
<link>
<name>app</name>
<type>2</type>
<locationURI>PARENT-2-WORKSPACE_LOC/sources/app/projectName</locationURI>
</link>
<link>
<name>common</name>
<type>2</type>
<locationURI>PARENT-2-WORKSPACE_LOC/sources/common</locationURI>
</link>
<link>
<name>drivers</name>
<type>2</type>
<locationURI>PARENT-2-WORKSPACE_LOC/sources/drivers</locationURI>
</link>
<link>
<name>hal</name>
<type>2</type>
<locationURI>PARENT-2-WORKSPACE_LOC/sources/hal/ev-build</locationURI>
</link>
<link>
<name>modules</name>
<type>2</type>
<locationURI>PARENT-2-WORKSPACE_LOC/sources/modules</locationURI>
</link>
<link>
<name>rtos</name>
<type>2</type>
<locationURI>PARENT-2-WORKSPACE_LOC/sources/rtos</locationURI>
</link>
</linkedResources>
</projectDescription>
Best Regards,
Pavel
2020-04-29 2:13 AM
Hello.
I finally solved this problem.
Here's how for everyone with the same issue:
1) Go to Project->Properties.
2) Search for indexer.
3) Set to this setting:
4) Rebuild index.
I don´t know, what setting is responsible for fixing this issue, but everything is working now, and this is what is important for me.
Thank you all for help.
Best Regards,
Pavel