cancel
Showing results for 
Search instead for 
Did you mean: 

Where is RTOS avare debugging from the Atollic Studio?

PJank.1
Associate

You have hided most interesting pluigins Atollic has like RTOS avare debugging and hard fault analyzer. There is no J-Link support. All the easy avaiable views in atollic are now hidden. What is going on?

4 REPLIES 4
Markus GIRDLAND
ST Employee

RTOS aware debugging is on the road map but has not been transferred over from TrueSTUDIO yet, other features has gotten priority.

There is J-Link support but it's sometimes filtered in version 1.1.0 (will be fixed in the next release), what target are you trying to debug?

Some perspectives has gotten a different layout and default views but it should be easily customized.

Stefano Oliveri
ST Employee

If you use FrreeRTOS then you can try the state-viewer plugin from this web page:

https://www.highintegritysystems.com/tools/stateviewer/

It provides the Task, Queue and Timer views.

0690X00000BvidjQAB.png

Maybe I am wrong but 99% of the professional developers use some kind of RTOS. And you give it a low priority. Bizarre

The problem is that there is no way to pass correct command line options or commands to the gdbserver. BTW why did you hide from the debug perspective HF analyser ?