2021-10-08 8:44 PM
Failed to execute MI command:
load "G:\\udemy\\embedded c\\my_workspace\\target\\001HelloWorld\\Debug\\001HelloWorld.elf"
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load "G:\\udemy\\embedded c\\my_workspace\\target\\001HelloWorld\\Debug\\001HelloWorld.elf"
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load "G:\\udemy\\embedded c\\my_workspace\\target\\001HelloWorld\\Debug\\001HelloWorld.elf"
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation ""
2. here is console output "" STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
Encountered Error when opening C:\ST\STM32CubeIDE_1.6.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.6.0.202101291314\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down... ""
2021-10-09 3:19 AM
STM32CubeIDE is built upon Eclipse and uses gnu tools (linux like) under the hood. All path specs will be transformed between Windows style, Linux style and whatever style else. So, the golden rule is: do not use spaces, umlauts, and other "difficult" characters for the path of your project. Keep it short and use letters and digits only. I spotted a space in "embedded c" in your path. I know, such a rule sounds stupid in 2021, but...
happy programming
KnarfB
2021-10-12 10:03 PM
I did not use spaces, umlauts and other "difficult character " for the path of my project. but still this problem occurse. please help me for this.
2021-10-12 10:57 PM
Hmm,
you did in the above screen dumps.
load "G:\\udemy\\embedded c\\my_workspace\\target\\001HelloWorld\\Debug\\001HelloWorld.elf
definitely containes a space char " ". If you have changed that, show the new error with its Details.
Here are some common pitfalls/suggestions:
hth
KnarfB
2022-05-04 3:36 AM
Hello,
I have exactly the same problem. Have you found a solution to this problem?
Thanks in advance.