cancel
Showing results for 
Search instead for 
Did you mean: 

What is the point of this UI element?

capnhyaku
Associate
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

I realize this post is more a rant than a question seeking a solution, but the point of the element is to include the C++ compiler in the project. Files still need to be named appropriately for it to be treated as a C++ file. If that's not checked, and you have *.cpp files in your project, it won't know what to do with them.

If you feel a post has answered your question, please click "Accept as Solution".
Semer CHERNI
ST Employee

Hello @capnhyaku 

First let me thank you for posting.

The STM32CubeMX (the code generator) does not generate C++ code it only generate C code.

However, like @TDK  have mentioned, the this check box is used to include C++ compiler in the project in case your project will contain C++ code.
For example, if you are planning to use TouchGFX for graphics you need to check this box as TouchGFX will generate C++ code.

BR,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.