2024-04-11 6:35 AM
Hi,
I had previously set up a USB serial communication that has been working with multiple STM32 types and in multiple projects. With the latest update to STM32CubeIDE Version: 1.15.0 Build: 20695_20240315_1429 (UTC) I had a problem.
Problem: unassigned variable warnings in USB_DEVICE/App/usbd_desc.c when tried to build the project. The project runs but the COM port number changes with each restart of the MCU which is very inconvenient for practical use.
Workaround: In the file USB_DEVICE/App/usbd_desc.c edit the routine starting to replace the missing commands as per below.
I hope this helps. Maybe it could be fixed in a new release.
H.
/**
* @brief Create the serial number string descriptor
* @param None
* @retval None
*/
static void Get_SerialNum(void)
{
uint32_t deviceserial0;
uint32_t deviceserial1;
uint32_t deviceserial2;
deviceserial0 = *(uint32_t *) DEVICE_ID1; // Missing
deviceserial1 = *(uint32_t *) DEVICE_ID2; // Missing
deviceserial2 = *(uint32_t *) DEVICE_ID3; // Missing
deviceserial0 += deviceserial2;
if (deviceserial0 != 0)
{
IntToUnicode(deviceserial0, &USBD_StringSerial[2], 8);
IntToUnicode(deviceserial1, &USBD_StringSerial[18], 4);
}
}
/**
Solved! Go to Solution.
2024-05-02 3:39 AM
Hello @HWhit.1
This issue was fixed in CubeMX6.11.1 which is already published in the st.com
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-11 6:53 AM
Hello @HWhit.1
Thank you for reporting this. I think you are tooking about the same issue reported on this post which has been reported internally to the Dev team (under internal ticket number 177153) to correct it ASAP. Thanks again for reporting.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-02 3:39 AM
Hello @HWhit.1
This issue was fixed in CubeMX6.11.1 which is already published in the st.com
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.