2024-12-12 5:34 AM - edited 2024-12-12 7:30 AM
Hello,
I am using the STM32G070RB and can start the bootloader. I am sending the command get checksum 0xA1 + 0x5E but I receive a NACK Byte directly after that. So I assume that this has to do with the protection active, since the flow diagram in the AN3155 shows only this path.
So in order to fix this issue I was thinking to send the readout unprotect command first and then the get checksum command. I did this but it doesn't work either.
Please note that I pull the Boot0 Pin high again an I am able to start the bootloader again after the reset caused by readout unprotect command.
Any help would be appreciated
2024-12-12 5:40 AM
Hello @crisay794266 ,
Can you precise the bootloader version of MCU this can be done by checking the bottom right window when connecting via CubeProgrammer.
Regards
2024-12-12 5:47 AM
It is 0xB2
2024-12-12 11:48 AM
Run the GET COMMAND command to see if the get checksum command is supported.
I recall them leaving out some commands due to space on the smaller chips.
2024-12-12 1:24 PM
Presumably if you unprotect the memory, it will mass-erase the content, so not going to be helpful to checksum content.
As TDK indicates you should be able to get the loader to enumerate the supported commands.