2021-03-22 7:16 AM
Hi all,
I'm using STLink V2 (Not STLink V2 ISOL) to program and debug a STM32F103C8 microcontroller(Development board is a low cost STM32 bluepill). Programming and debugging via SWD works like a charm, without any issue. But I was never able to get the JTAG working. I made all the pin connections according to page 12 of UM1075. The way I tried is given below.
And that's all.
When I try to debug I get the message "Failed to Start GDB server" along with
"Error in initializing ST-LINK device." and "Reason: No device found on target." messages on console. But when I select SWD as debug interface, it works fine.
Any thoughts about this? What am I missing?
Solved! Go to Solution.
2021-03-22 8:29 AM
A real ST-LINK/V2 ?
Assuming as SWD works that VTarget is present.
Still sounds like a pin connectivity is, from pod, to IC pin. Check schematic. If wired correctly not reason I can see why it wouldn't work.
Enumerate exact what you've connected to what, not just refer to another document. List what you've done, and perhaps attach a clear/focused picture of the implementation.
All HAL related remaps, etc could be sidestepped if BOOT0 is pulled HIGH
2021-03-22 8:29 AM
A real ST-LINK/V2 ?
Assuming as SWD works that VTarget is present.
Still sounds like a pin connectivity is, from pod, to IC pin. Check schematic. If wired correctly not reason I can see why it wouldn't work.
Enumerate exact what you've connected to what, not just refer to another document. List what you've done, and perhaps attach a clear/focused picture of the implementation.
All HAL related remaps, etc could be sidestepped if BOOT0 is pulled HIGH
2021-03-23 7:52 AM
@Community member Thank you for your reply.
Since you mentioned about pin connectivity, I checked it.
Of course it was a lousy connection. I fixed it. Now JTAG works fine.
(Yes, My STLink/V2 is a real one. And BOOT0 is pulled low.)
Regards,
Kasun