2024-12-17 5:10 AM - edited 2024-12-18 5:10 AM
I've been trying several days to just get any project up and going for the STM32WBA52GU. As soon as I add the WPAN middleware, the HAL definitions go haywire with errors when I compile it. I've tried following tutorial in the wiki with documentation, but nothing seems to be working. I can import an example for the Nucleo WBA55, and it will compile. However, using the same settings for a new project fails (even when trying to target the WBA55). Any help would be appreciated. I'm using STMCubeIDE 1.17.0 with the latest firmware libraries.
786 | HAL_StatusTypeDef HAL_RCCEx_PeriphCLKConfig(const RCC_PeriphCLKInitTypeDef *PeriphClkInit);
| ^~~~~~~~~~~~~~~~~
| HAL_CRC_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rcc.h:2452:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_CRC_StateTypeDef'?
2452 | HAL_StatusTypeDef HAL_RCC_DeInit(void);
| ^~~~~~~~~~~~~~~~~
| HAL_CRC_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rcc.h:2453:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_CRC_StateTypeDef'?
2453 | HAL_StatusTypeDef HAL_RCC_OscConfig(const RCC_OscInitTypeDef *RCC_OscInitStruct);
| ^~~~~~~~~~~~~~~~~
| HAL_CRC_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rcc.h:2454:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_CRC_StateTypeDef'?
2454 | HAL_StatusTypeDef HAL_RCC_ClockConfig(const RCC_ClkInitTypeDef *RCC_ClkInitStruct, uint32_t FLatency);
| ^~~~~~~~~~~~~~~~~
| HAL_CRC_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rcc.h:2491:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_CRC_StateTypeDef'?
2491 | HAL_StatusTypeDef HAL_RCC_GetConfigAttributes(uint32_t Item, uint32_t *pAttributes);
| ^~~~~~~~~~~~~~~~~
| HAL_CRC_StateTypeDef
In file included from ../Core/Inc/stm32wbaxx_hal_conf.h:279:
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:89:3: error: unknown type name 'HAL_LockTypeDef'
89 | HAL_LockTypeDef Lock; /*!< RNG locking object */
| ^~~~~~~~~~~~~~~
In file included from ../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:287:
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng_ex.h:221:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
221 | HAL_StatusTypeDef HAL_RNGEx_SetConfig(RNG_HandleTypeDef *hrng, const RNG_ConfigTypeDef *pConf);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng_ex.h:222:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
222 | HAL_StatusTypeDef HAL_RNGEx_GetConfig(RNG_HandleTypeDef *hrng, RNG_ConfigTypeDef *pConf);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng_ex.h:223:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
223 | HAL_StatusTypeDef HAL_RNGEx_LockConfig(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng_ex.h:232:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
232 | HAL_StatusTypeDef HAL_RNGEx_RecoverSeedError(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:296:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
296 | HAL_StatusTypeDef HAL_RNG_Init(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:297:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
297 | HAL_StatusTypeDef HAL_RNG_DeInit(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:318:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
318 | HAL_StatusTypeDef HAL_RNG_GenerateRandomNumber(RNG_HandleTypeDef *hrng, uint32_t *random32bit);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:319:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
319 | HAL_StatusTypeDef HAL_RNG_GenerateRandomNumber_IT(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:369:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
369 | HAL_StatusTypeDef RNG_RecoverSeedError(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
In file included from ../Core/Inc/stm32wbaxx_hal_conf.h:283:
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rtc.h:205:3: error: unknown type name 'HAL_LockTypeDef'
205 | HAL_LockTypeDef Lock; /*!< RTC locking object */
| ^~~~~~~~~~~~~~~
In file included from ../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rtc.h:732:
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rtc_ex.h:1487:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RTCStateTypeDef'?
1487 | HAL_StatusTypeDef HAL_RTCEx_SetTimeStamp(RTC_HandleTypeDef *hrtc, uint32_t TimeStampEdge, uint32_t RTC_TimeStampPin);
| ^~~~~~~~~~~~~~~~~
| HAL_RTCStateTypeDef
2024-12-19 7:43 AM
Hello @JLReyno ,
First let me thank you for posting and welcome to the ST Community.
Your request is under investigation, and I will get back to you ASAP
Thanks.
Mahmoud
2024-12-19 10:06 AM
Thanks, Mahmoud! To keep you up to date with my latest work, I've tried some other advice and started with the P2P_server example for the WBA55 and then modified it for the WBA52. I can get it to compile, but the BLE stack fails to initialize (line 1081 in app_ble.c). I've attached that project for reference if that is any help.