cancel
Showing results for 
Search instead for 
Did you mean: 

Transfer code from IAR to CubeIDE?

TNils.1
Associate II

Hi

I have been requested to redesign a current product using an ST32F405RG where the software was developed in the IAR IDE.

This is mainly a HW update that requires only a little bit of SW changes.

Unfortunately the IAR IDE is not available. Hence, I wonder if it is possible/feasible to use/transfer the code/files from the IAR environment and use them in ST's CubeIDE?

If possible, how cumbersome can I expect it to be?

Thanks!

3 REPLIES 3
TDK
Guru

> If possible, how cumbersome can I expect it to be?

It should be quite manageable.

If you feel a post has answered your question, please click "Accept as Solution".
TNils.1
Associate II

Great, thanks!

TNils.1
Associate II

If it hadn't been for the great mess in the original files, migrating via Atollic Truestudio made it very manageable ;)