2021-03-31 9:22 AM
I'm working on a project that requires very strict control of the toolchain itself. We must specify exact versions of toolchain components as part of our documentation and production process.
The problem I'm having is we started work at Stm cube ide 1.4.0, which was later patched to 1.4.2. My team updated their installs through the IDE's integrated update service. But now I need to bring a few new development PC's online with identical toolchains. I can download 1.4.0 from the website, but I cannot find this patch anywhere.
Is this patch available for download? Is it on a server somewhere? How long is it guaranteed to remain accessible?
If I can't get this patch as a download, what would you recommend for an application like mine where strict control of the toolchain version must be maintained for a long time (potentially *decades*). Should I stick to downloadable major releases only?
Solved! Go to Solution.
2021-04-07 6:05 AM
Hi @Dfarr.1 ,
We have a commitment to deliver "full installers" for all future CubeIDE releases.
So in the specific case of 1.4.1 and 1.4.2 only "P2" ONLY online patches are available and user has to rely on 1.4.0 full installer.
Is it possible to host the p2 patches on LAN? Well conceptually we should be able to do so as a zip-file. But we don't provide such zip-files today.
2021-04-06 10:28 AM
Have a look to https://www.st.com/resource/en/user_manual/dm00603964-stm32cubeide-installation-guide-stmicroelectronics.pdf
Consider Chapter 6: Update an STM32CubeIDE installation
2021-04-06 11:05 AM
Thanks, that answers the question of setting up my new development machines this time.
How long are these updates guaranteed to be available from the STM update server like this?
Can the update files from this server be stored offline and referenced (on a LAN for example) using a similar process be pointing eclipse at a LAN server rather than the STM updatesite1 server?
2021-04-07 6:05 AM
Hi @Dfarr.1 ,
We have a commitment to deliver "full installers" for all future CubeIDE releases.
So in the specific case of 1.4.1 and 1.4.2 only "P2" ONLY online patches are available and user has to rely on 1.4.0 full installer.
Is it possible to host the p2 patches on LAN? Well conceptually we should be able to do so as a zip-file. But we don't provide such zip-files today.