2020-12-04 01:21 AM
2021-02-06 10:46 PM
Hi Mattias.
Everything was working fine till now with the Version 1.5, till today - however today when I started to debug, the same problem has now started with Ver 1.5 also. I get exactly the same message as the screenshot given earlier in my thread.
"An internal error occurred during: "Launching SensorNodeV4 SN103".
java.lang.NullPointerException"
I am seriously at a loss what to do. Please help!
2021-02-24 04:30 AM
Did you "today" (17 days ago) also make another Update of CubeIDE? Is it working?
In case of problems a new full re-install is the best bet. The update mechanism has some known issues:
People "should" not run into these kind of issues. If you do, then consider a full re-install. Only takes 5-10 minutes. Yes - annoying as #¤%&*... but better then being stuck. And your workspaces and projects are not touched by the re-install so there should be minimal re-configuration of the tool!
2021-02-24 10:47 PM
Hi Mattias
Yes, I ran into the same issue again 18 days ago, but thankfully sorted it out with some struggle spanning over days, in which I got a bit fed up with the complexities in CubeIDE and decided to change over to KEIL uVision, which is much simpler to use for a starter like me.
Thanks for the interest..
Naveen
2021-02-25 04:03 AM
Hi Mattias
5 hours ago I messaged you that I solved the problem by reconfiguring the Debug Profile.
It seems I was wrong. The error is happening again, DESPITE changing the Debug Profile!!
Stuck Again!!
Pl help!
NA
2021-03-01 05:43 AM
Hi,
Yes, the learning curve for CubeIDE is a bit steeper than for some other IDEs. Some things could be simplified wil other things are a balance simplicity vs flexibility. In those cases we tend to go for flexibility as a first step, and if later required we can try to add layers on top to simplify stuff...
Anway, just to come back to you 3 points:
Well good luck in Keil, and welcome back should you later want to switch back ;-)
2021-03-01 07:57 PM
Hi Mattias
Many thanks for your response which I truly appreciate. Based on your advice, I tried to work again on the STM32CubeIDE, but soon ran into a number of difficulties! But first, to answer your Point 3 on reset: I meant that when I press the RESET button (Not Terminate and relaunch), it goes through the cycle of re-compiling and reloading the program before reverting to the Debug mode. Whereas actually I simply want to re-run the loaded program only. This is so in most of my earlier IDE experiences with Microchip as also KEIL.
Is there a setting which simply resets the pre-loaded program to start?
Now the fresh issues:
Shall I raise a new ticket for this new issue?
N
2021-03-02 07:34 AM
Hi N,
About reset vs terminate and re-launch. I better check that we are talking about the same thing here :)
About the fresh issues: