cancel
Showing results for 
Search instead for 
Did you mean: 

Target not found on cubeide

MSadf.1
Associate II

0693W00000aJJfaQAG.pngI'm working with a stm32 nucleo H723ZG board. Until yesterday everything worked fine, I could program the board and everything worked well. When I tried to connect my board to my PC today, cubeide could not find the board when I tried to run my program. I did not change any settings. The COM led stays red ( ld4 led ) and the ld6 led stays red aswell and no other leds are on. I tried to erase everything with the cube programmer but I got the error no target found when I tried to connect. here the text I got.

10:59:26 : ST-LINK SN : 001D00443438511734313939

 10:59:26 : ST-LINK FW : V3J11M3

 10:59:26 : Board    : NUCLEO-H723ZG

 10:59:26 : Voltage   : 0.00V

 10:59:26 : No STM32 target found!

 10:59:26 : ST-LINK SN : 001D00443438511734313939

 10:59:26 : ST-LINK FW : V3J11M3

 10:59:26 : Board    : NUCLEO-H723ZG

 10:59:26 : Voltage   : 0.25V

 10:59:26 : Error: No STM32 target found!

6 REPLIES 6
gbm
Lead III

Try to change the Reset option to Hardware or to None.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

I already did that and it didn’t work

Peter BENSCH
ST Employee

When the voltage at the target is 0.25V and LD6 is lit, the NUCLEO-H723ZG draws more than 500mA from USB (see UM2407, section 6.6.1). You should check which additional devices you have connected to the NUCLEO.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

the board isn’t connected to anything

Well, I assume it's connected to a host with USB, right? ��

But if you haven't connected anything, you'd have to find out why the overcurrent detection has tripped. LD6 is controlled by U2 (STMPS2151STR), which switches CN1.1 (VBUS) to the signal 5V_USB_CHGR.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

On a conductive surface or conductive foam that might create a short-circuit, or regulator failure?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..