cancel
Showing results for 
Search instead for 
Did you mean: 

SWV Exception Timeline Graph - How to use?

PTiha
Senior

Hi!

I created a simple project in CubeIde to try out this function.

SWV Exception trace log works as it, but the timeline graph seems to me wrong.

Belong the debug session a moving vertical red line appears on the graph, and nothing else.

Could anyone help me?

0690X00000DXG7pQAH.png0690X00000DXG7fQAH.png0690X00000DXG7QQAX.png

6 REPLIES 6
PTiha
Senior

Hello,

Nobody has any idea what is the problem?

In Atollic this function is worked.

PTiha
Senior

Hi!

Has anyone else had similar experience with this program feature?

PTiha
Senior

Hello,

Since I can't accept not being able to use this feature, I did some additional tests.

Here are some screenshot from the debug session of test project.

You can see that there is no packet overflow or other issues during the trace.

The graph is totally useless. When I pause the debug session, I cannot scroll the trace log because eclipse refreshes it periodically.

0690X00000DYejVQAT.png0690X00000DYejQQAT.png0690X00000DYejLQAT.png0690X00000DYej6QAD.png

BOzge.1
Associate

Hi @PTiha​, did you solve this issue? I am having the same problem.

AWeie.1
Associate

Hi @PTiha​ , I am having exactely the same issue. Using SM32CubeIDE 1.5.1 on linux.

Did you find any solution to make it work?

PTiha
Senior

Sorry for the late answer! Unfortunately, there is no positive change. The function has been removed from the latest 1.6.0 CubeIDE, if I see it correctly ... There is nothing to say about this ... :(