cancel
Showing results for 
Search instead for 
Did you mean: 

strncpy_s in STM32: undefined reference to `strncpy_s'

OIp.1
Associate III

Hi. I have the following code:

messageprocesser.h

#ifndef INC_MESSAGEPROCESSER_H_
#define INC_MESSAGEPROCESSER_H_
 
#ifdef __cplusplus
extern "C" {
#endif
 
#include "main.h"
#include "usbd_cdc.h"
#include <stdint.h>
#include <string.h>
#include <stdio.h>
 
void process_Message(uint8_t* message, uint16_t Len);
void message_Received(uint8_t* message, uint16_t Len);
void send_Message(uint8_t* cmd, uint8_t* data);
 
#endif /* INC_MESSAGEPROCESSER_H_ */

messageprocesser.c

/*
 * messageprocesser.c
 *
 *  Created on: Jan 30, 2023
 *     Sorry for the dead code. I left it there so the error messages would make sense.
 */
 
#include "messageprocesser.h"
#include "main.h"
#include "usbd_cdc_if.h"
#include <string.h>
 
//Sample cmd: TOARM_FIRMV_00000000_4C\r\n
#define MESSAGE_LENGTH 25
#define COMMAND_CHAR 6	//See SW Protocol or sample cmd
#define COMMAND_LENGTH 5
#define DATA_CHAR 12
#define DATA_LENGTH 8
#define CHECKSUM_CHAR 21
#define CHECKSUM_LENGTH 2
 
void process_Message(uint8_t* message, uint16_t Len){
	HAL_GPIO_TogglePin(GPIOF, GPIO_PIN_10);
	unsigned char inputCmd[5];
	unsigned char inputMessage[8];
	unsigned char outputCmd[5];
	unsigned char outputData[8];
 
	//Function that separates message, inputCmd, and inputMessage.
 
//	strcpy((char*) inputCmd, (const char*)message + COMMAND_CHAR);
//	strcpy((char*) inputMessage, (const char*)message + DATA_CHAR);
	if (strncmp(inputCmd, "FIRMV", COMMAND_LENGTH) == 0){
		memcpy(outputCmd, "FIRMV", COMMAND_LENGTH);
		memcpy(outputData, "01050A00", DATA_LENGTH);
	}
	else{
		memcpy(outputCmd, "REEEE", COMMAND_LENGTH);
		memcpy(outputData, "99999999", DATA_LENGTH);
	}
 
//	message_Received(message, Len);
	send_Message(outputCmd, outputData);
}
 
void message_Received(uint8_t* message, uint16_t Len){
//	HAL_GPIO_TogglePin(GPIOF, GPIO_PIN_10);
	//CDC_Transmit_FS(message, Len);
//	uint8_t inputCmd[5];
//	uint8_t inputMessage[8];
 
}
 
void send_Message(uint8_t* cmd, uint8_t* data){
	uint8_t outputMessage[MESSAGE_LENGTH] = "TOWST_";
	strncpy_s((char*) outputMessage + COMMAND_CHAR, COMMAND_LENGTH, (const char*) cmd, COMMAND_LENGTH);
	outputMessage[COMMAND_CHAR + COMMAND_LENGTH] = '_';
	strncpy((char*) outputMessage + DATA_CHAR, (const char*) data, DATA_LENGTH);	//Why does having 2 strcats break the system?
//	strncpy((char*) outputMessage + DATA_CHAR, (const char*) '_', 1);
	outputMessage[DATA_CHAR + DATA_LENGTH] = '_';
	strncpy((char*) outputMessage + CHECKSUM_CHAR, (const char*) "27", CHECKSUM_LENGTH);
	outputMessage[23] = '\r';
	outputMessage[24] = '\n';
//	strcat((char*) outputMessage, (const char*) data);
//	strcat((char*) outputMessage, (const char*) '_');
//	uint8_t test_message[64] = "TOWST_VERAK_01050A00_27\r\n";
//	CDC_Transmit_FS(test_message, sizeof(test_message));
	CDC_Transmit_FS(outputMessage, sizeof(outputMessage));
}

The error and the warning:

../Core/Src/messageprocesser.c: In function 'send_Message':
../Core/Src/messageprocesser.c:56:2: warning: implicit declaration of function 'strncpy_s'; did you mean 'strncpy'? [-Wimplicit-function-declaration]
   56 |  strncpy_s((char*) outputMessage + COMMAND_CHAR, COMMAND_LENGTH, (const char*) cmd, COMMAND_LENGTH);
      |  ^~~~~~~~~
      |  strncpy
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: Core/Src/messageprocesser.o: in function `send_Message':
C:/Users/User/STM32CubeIDE/workspace_1.6.0/usbtest/Debug/../Core/Src/messageprocesser.c:56: undefined reference to `strncpy_s'

My understanding of strncpy_s is that it is a part of C11, and it is part of the string.h header file. I am unsure why my compiler does not consider strncpy_s as a valid preexisting operator.

My compiler is GNU11, so it should include C11 based on my understanding.

0693W00000YA3UPQA1.pngPlease let me know if more information is required.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

This function is defined in C11 Annex K, which is optional. Quoting from C11 (footnote 380 in Annex K):

Implementations that do not define _ _STDC_LIB_EXT1_ _ are not required to conform to these

specifications.

newlib does not appear to implement Annex K functions.

JW

View solution in original post

4 REPLIES 4
waclawek.jan
Super User

This function is defined in C11 Annex K, which is optional. Quoting from C11 (footnote 380 in Annex K):

Implementations that do not define _ _STDC_LIB_EXT1_ _ are not required to conform to these

specifications.

newlib does not appear to implement Annex K functions.

JW

Thank you. Is there a setting I could configure, or external file I could place within my project to implement Annex K?

waclawek.jan
Super User

Sorry, I don't use or even know any, and whatever I find using google you probably already know...

JW

Please see here and here