Strings in RAM and Flash and transfer them to function
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-09 12:14 AM
Hi
How can I put strings in fash memory in gcc compiler so that there is no copy in both memories. In 8bit AVR we need to use PROGMEM . How it is in STM32 gcc?
The secong thing. If i have for example such a function void MyFunction( char *Stri(ng); which accepts pointers to string and if i call this function with this parameter MyFunction("String to Pass"); Where this string beeing a parameter of this function will be placed? In Falsh, in RAM or mybe it will be two copies in Ram and Flash?
- Labels:
-
STM32CubeIDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-09 1:11 AM
ARM cortex and AVR have different architecture.
AVR is Harvard: separate memory for data and instructions.
ARM Cortex is von Neumann : only one memory.
So to put a string in Flash you must use the const qualifier:
const char str [] = "abc" ;
If you use :
char str2 [] = "xyz" ;
then the string will be in Flash and copied to RAM by the startup code, before the call to main().
If you use MyFunction("String to Pass"); then the string is const and placed in Flash.
Beware: if you use
MyFunction (str) ;
the compiler will warn about const qualifier, if the function declaration is:
MyFunction(char *) ;
So you must declare:
MyFunction (const char *) ;
Have a nice day.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-09 2:37 AM
Thank you for detailed explanation.
As I understood i can not have one function suport two kind of strings? I mean: do i need to have one function to work with const strings and one with those in ram?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-09 5:23 AM
You can cast the 'const char *' to 'char *. Not very clean but doable.
MyFunction ((char *) str) ;
But MyFunction cannot modify the string, as it is in Flash.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-09 12:10 PM
Tank you very much for help :grinning_face:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-10 11:34 AM
Welcome to the wonderful world of 32bit ARMs. One of the nice things about stm32s is the flat 32bit ​(4 GB) address space which is, not coincidentally i believe, the same size as the data bus width. The nice thing about this is the ease of using pointers in C as a pointer and uint_32 are essentially the same thing, just used differently by the compiler. There is nothing "unclean" about casting from a const uint_8 * to a uint_8 * as they not really different (except not being able to write directly to flash). It is a formality to keep the compiler quiet. It's incredibly flexible and powerful, a true paradise for a traditional C programmer.