2024-08-25 03:31 AM
Hi,
I cannot login to myST. When I press myST|login nothing happens, no window with prompt for credentials appears.
Because of that I cannot manage and download firmware packs. Code generation does ton work. Generated project is incomplete and cannot be build.
STMCubeIDE version: 1.16.0.
Regards,
Piotr Romaniuk
Solved! Go to Solution.
2024-09-01 09:13 AM
@Piotr Romaniuk Windows 7 is not a supported OS for CubeIDE anyway (per the installation guide).
Microsoft's Edge browser on Win10/11 is compatible with Chrome, it should just work.
Linux is, as always, an exciting land of freedom. Everyone can choose freedom or productivity))
2024-09-01 09:44 AM
Hi Pavel,
Thank you for additional clarification.
I hope that:
- 'should just work' means 'will just work',
- 'or' is in the logic sense, so it can be achieved both 'freedom and productivity'. Otherwise it looks like accusation that Linux is not productive.
By the way, do you know what is the rationale for this trend - creating applications in HTML+CSS+JavaScript ? I see this not only in the ST environment.
Regards,
Piotr Romaniuk
2024-09-01 12:44 PM
Yes, Edge just works, at least on Windows. (the modern Edge based on Chromium, not the ancient Microsoft's one named Spartan).
2024-09-01 08:15 PM
Hello,
"3. Point to the manually downloaded zip file, then accept the license and install it"
Indeed it can be done manually without log in into myST in stm32cubeIDE, here is the instruction:
Regards,
Piotr Romaniuk