cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4使用STM32cubeIDE输出浮点数,程�?会进入硬件错误。

超哥
Associate II

勾选了设置中的输入输出浮点,�?然无效。修改为标准库或者精简库也无效。网上也有很多人�?�到了这样的问题。请问怎么解决?官方有解决方案�?�?官方是�?�会在�?�期的版本中解决掉这个问题?

4 REPLIES 4
Imen.D
ST Employee

Hello,

Please ask your question in English.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
超哥
Associate II

Stm32f4 uses stm32code ide to output floating-point numbers, and the program will enter a hardware error.

Setting the input and output floating-point options is also invalid. Changing to a standard or thin library is also not valid. There are also many people on the Internet who have encountered such problems. How can I solve it? Is there an official solution? Will the official fix the problem in a later version?

All methods have tried or can't print floating-point numbers