cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE V1.15.1 slow build process

zmiga
Associate II

Hello everyone,

I've just updated cubeIDE from V1.14.x to V1.15.1 and duration of build process on the same project increased by around 4x.  

With V1.14 it took around ~10s, now with V1.15.1 takes ~40s to build the same project on the same machine. 

 

Is that a known issue? How can I mitigate that?

 

Thank for your help!

BR, Žiga

3 REPLIES 3
Souhaib MAZHOUD
ST Employee

Hello @zmiga 

Could you provide your project in order to investigate the issue.

BR

Souhaib

Hi Souhaib, 

unfortunatelly not, because it contains propriatery code. 

 

 

What do you recommend for me? Should I downgrade to V1.14 version?

Are there any general tricks to speed up the build process?

 

Thank you!

BR, Žiga

I've downgraded to V1.14.1 and it compiles in less than 10 sec. Seems to be some specific problem with my PC setup and Cube V1.15 🤔

 

Additional info about the PC I'm using:

OS Version: 10.0.19045 N/A Build 19045
OS Manufacturer: Microsoft Corporation
OS Configuration: Member Workstation
System Manufacturer: Dell Inc.
System Model: OptiPlex 5060
System Type: x64-based PC

Processor(s): 1 Processor(s) Installed.
[01]: Intel64 Family 6 Model 158 Stepping 10 GenuineIntel ~3192 Mhz
BIOS Version: Dell Inc. 1.29.0, 29. 02. 2024

BR, Žiga