2022-03-05 05:05 PM
Hi
When I try to open the .ioc file associated with my project from within the STM32CubeIDE, I get the following error:
Invalid Input: 'FreeRTOS_Test_001.ioc' file content is not supported.
This file has been generated with STM32CubeMX version '6.4.0'.Your current STM32CubeMX version is '6.3.0'.
Please check for update: Help > Check for Updates
CubeIDE is obviously pointing to an older version than the version CubeMX version (6.4) that I opened from my desktop to create the project in the first place.
How can I fix this?
Best regards
Rob
Solved! Go to Solution.
2022-03-07 05:44 PM
I don't think it is connectivity. I run updates from CubeIDE regularly. At least once per day.
In any event I downloaded 1.8 and have got it working.
2022-03-05 05:43 PM
What is your CubeIDE version? Latest is v1.8.0.
2022-03-05 06:11 PM
Ahh! Good question! My IDE is 1.7.
I have tried to update the IDE from within the IDE, Help->Check for updates, but it comes back "No Updates Found"
What do I have to do to update my STM32CubeIDE to the latest? Uninstall - download and then install the updated one?
Regards
Rob
2022-03-05 08:02 PM
2022-03-07 05:44 PM
I don't think it is connectivity. I run updates from CubeIDE regularly. At least once per day.
In any event I downloaded 1.8 and have got it working.
2022-03-08 01:19 AM
Could you try in your CubeIDE 1.7.0 installation to do this:
Window > Preferences > Install/Update > Available software sites
Try to Reload, the marked three update sites:
Any error message?