2019-10-07 02:56 AM
Hi there,
I'm using STM32Cube Ide to work wih my STM32F7.
I really like this software also for the integration of STM32CubeMX.
I use the STM32CubeIde to configure the hardware, peripheral, OS and so on but when I build the configuration I noticed that also the Include Path are restore.
So every time I change a perpheral setting and I rebuild the the project, the project lost the setting and I need to add manually every source folder that I added.
Is there a way to avoid this?
Thanks for the help.
BR,
Federico
2019-10-15 11:59 AM
Definitively a bug.
Sounds some improvements have been done Thanks STM32CubeIDE V1.1.0 just released on st.com
2019-11-07 08:57 PM
For me, 1.1.0 has problems on MacOS. I cannot get ST-Link debug to work, only OpenOCD. 1.0.2 works fine (except the bug above, very annoying!) These tools are rather disappointing.
2019-11-08 12:07 AM
"1.1.0 has problems on MacOS" what do you mean ? Is such still related to "resets include paths when build hardware project" i.e. your post header or MacOS issues in general relying on 1.1.0. If general 1.1.0 MacOS issue I obviously agree according numerous post about.
2019-11-11 11:27 AM
I have the same problem as OP, and in addition, on MacOS, the ST Link debugging doesn't work. It does work on 1.0.2