2019-05-07 6:20 AM
Hello,
I downloaded STM32CubeIDE v1.0.0 and tried to install it on my Windows 7 computer.
Unfortunatly I have a NSIS Error "Error launching installer". I tried to download again the file, tried on another windows 7 PC but I still have this issue.
Someone know how to solve this issue?
Thanks and best regards
Fabien
Solved! Go to Solution.
2020-01-12 5:08 AM
Same here, in Jan 2020 on Win10 64bit;
2019-05-07 10:43 AM
Hello! Windows 10 also has a startup problem!
2019-05-08 8:09 AM
As a first step please make an md5sum check using the following MD5:
c1004055082e06392ea358ed796060c8
As a second step given that the first step is OK. Please check your anti-virus software log files to make sure it doesn't interfere with the launching of the installer. Please share your findings with us!
2019-05-09 12:23 AM
Thanks for your answer but unfortunately installation still fail.
I checked the MD5 of the .exe file and it match.
I disabled my anti-virus software (Microsoft Security Essentials) but I still have the NSIS error during installation.
2019-05-13 4:12 AM
Are you launching from a USB stick or something similar? Do the two different PCs have the same setup? With network and anti-virus software? Are the computers 32 or 64-bit?
I've tried reproducing the error on a few of my windows computers that are on different networks with different setups but no NSIS error so far. Any specific tips to help in how I can reproduce would help a lot!
2019-05-14 5:04 AM
The software is on my hard drive.
Please find a summary of my tests:
I also discover that if I unzip the file with windows embedded zip, the MD5 match with the one you provided to me. But, if I unzipped it with 7-zip software the MD5 doesn't match.
So I used always the file with the correct MD5 for all these tests.
2019-05-16 2:37 AM
This is very unusual and I can't seem to reproduce it.
The fact that the Windows 7 SP1 Pro 32 bits isn't working isn't a huge deal since we only support 64 bit installers. However, you should receive a dialogue explaining that instead of an NSIS error.
I tried using the installer with Windows 7 SP1 Pro 64 bit here in the office, both with and without antivirus active, and it worked both times.
Does the path to the installer contain any non-ascii characters?
Can you place the installer right in C:/st-stm32cubeide_1.0.0_2872_20190423-2022_x86_64.exe and see if it makes a difference?
2019-05-16 3:19 AM
Thanks a lot for your help, all is working well.
Your idea was correct, the issue came from the path. In my case it was D:\Téléchargement\STM32CubeIDE
About Windows 7 32bit, the issue was an NSIS corruption file. The corruption came during unzip process. With a good .exe file, I have the correct dialogue box.
Do you have an idea about corrupted file when I used 7-zip software?
2019-06-26 4:21 PM
2019 and STILL with problems with accented vowels!!?? Really??
I had the same issue, and of course the installer said nothing in order to get a clue... pitiful >:(
2019-08-02 6:47 AM
I ran into this too, and I found a solution like this:
1. Reduced the name of the folder and file to stm32cubeide_1.0.2
2. Moved the folder to the root of drive D, before it was in a folder with a name in Russian.
3. Disable 360 Total Security.
4. I use it!
Win10 Pro x64