2022-10-09 12:53 PM
Software:
Version: 1.10.1
Build: 12716_20220707_0928 (UTC)
When I use the Memory Browser and display 32 bits wide, and hover my mouse over the LSB, it shows as at address 0x2001FFE3
But, if I change the display to 8 bits wide, it clearly shows the LSB at 0x2001FFE1
Surely both should show 0x2001FFE1
Both are set to "Little-endian"
2022-10-27 01:23 AM
Hi @JJaco.8 and welcome to the Community 🙂,
For my side it is not a bug it is the principle of little Endia format.
The difference between the Big-endian and the little endian is descripts in the below table.
The difference between the 32 bits and 8 bits wide representation in the little-endian format is find in the below tables:
For more explanation I advise you look at this link.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Thank you
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.