cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE Line Numbers Glitching

Adsehgal
Associate

Hi,

I am not sure if this is the right forum category to post this to, but I have noticed CubeIDE keeps messing up the line numbers, and this has quite often usually when I use CMD+F to find something or when I fold/unfold a function... And the only way to fix it is by closing that file and opening it again. Does anyone have any idea why this happens or if there is a workaround? I have noticed this happen on multiple versions of the IDE, I am currently running 1.6.1, also installed is the Darkest Dark theme, though I have noticed this happens without any theme as well.

Thank you!

0693W00000D26HsQAJ.png

2 REPLIES 2
TDK
Guru

What OS are you using? I've never seen this on Win10. I've seen other visual issues, but not this.

If you feel a post has answered your question, please click "Accept as Solution".

Im running MacOS 11.4 Big Sur