2021-01-02 06:25 AM
I had several versions of the IDE installed on my machine but none of them could connect to the internet to update or load code. I keep getting the error message "In order to benefit from best experience a network connection is required. Do you want to set connection parameter now?". At first I thought it was because Norton was blocking the the applications through the firewall but I uninstalled Norton and installed the IDE again but that didn't fix the problem. I installed the IDE on my brothers machine which doesn't have Norton and it worked fine on there. I also have used different networks in the past 2 months so that cant be it. Can anyone please help?
2024-01-11 02:32 PM
I had the same problem and solved it by changing Active Provider to Direct.