2021-07-12 10:39 PM
Hello,
Right now the IDE is driving me crazy: I've written an include in my project, made requred/mandatory entry in project settings (see the attachement), and get the error message "No such file or directory" when I compile the project.
I've checked several times that everything is correct, can't find any errors, but I always get this error message.
As you can see in the bottom part of the screen shot, the compiler doesn't include this directory ("-I ...") in the command line.
Can someone help me please!
Thanks in advance,
Michael
Solved! Go to Solution.
2021-07-12 11:06 PM
Hello @Mick P. F. ,
As indicated by your screenshot, you've set the assembler include paths not the compiler's.
Best regards,
@SBEN .2
2021-07-12 11:06 PM
Hello @Mick P. F. ,
As indicated by your screenshot, you've set the assembler include paths not the compiler's.
Best regards,
@SBEN .2
2021-07-13 12:24 AM
I'm very sorry!!!
My (serious) illness causes severe pain, which in turn leads to constant stress.
I checked and checked it several times!
That's how I make such simple mistakes.
Many thanks for your help!
Kind Regards,
Michael
2021-07-13 12:39 AM
Hello @Mick P. F. ,
No issue Mick, we're here to help. And it happens to the best of us.
Hope you get well soon!
Best regards,
@SBEN .2
2021-07-13 1:04 AM
Many thanks,
the disease cannot be cured.
Because of that, I can not work anymore and continue to do it as a hobby, which I did professionally until 2 years ago.