STM32CUBEIDE DEBUG PROBLEM
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-15 1:06 AM
Hello
My debugger is shutting down after downloading code into chip
I can connect STLINK UTILITY and uploading code hex files properly
STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.7.0-RC1
-------------------------------------------------------------------
ST-LINK SN : 50FF6D064965575354401887
ST-LINK FW : V2J37S0
Board : --
Voltage : 2.89V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x445
Revision ID : Rev 1.0
Device name : STM32F04x/F070x6
Flash size : 32 KBytes
Device type : MCU
Device CPU : Cortex-M0
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a14724.srec
File : ST-LINK_GDB_server_a14724.srec
Size : 27540 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 26]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.764
Verifying ...
Download verified successfully
Debugger connection lost.
Shutting down...
Labels:
- Labels:
-
DEBUG
-
STM32CubeIDE
-
STM32F0 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-15 11:50 PM
Is there any recommendation ?