2025-07-23 6:40 AM - last edited on 2025-08-01 3:11 AM by Andrew Neil
Hello all.
Im starting to work with the Nucleo L476RG board and am now at the stage i would like to bring up the CAN bus. I haven noticed there are CAN bus examples available for other Nucleo baords but not in the current STM32Cube_FW_L4_V1.18.1 for the L476. Is this available or been ported to the L476?
Many thanks
Rich
2025-08-01 3:00 AM
Hello @Rich_P and welcome to the community;
I recommend you referring to these examples and get inspired to configure CAN bus:
- STM32CubeL4/Projects/STM32L476G-EVAL/Examples/CAN/CAN_Networking at master · STMicroelectronics/STM32CubeL4 · GitHub This example runs on STM32L476xx devices and it has been tested with STM32L476G-EVAL board and can be easily tailored to any other supported device and development board.
- Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 1) - STMicroelectronics Community
- Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 2) - STMicroelectronics Community
I hope this help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-22 8:37 AM
Hello @Rich_P ,
Are these resources can help you to start CAN with Nucleo-L476RG board?
Note that the CAN_Networking example runs on STM32L476xx devices.
If your request is answered, please click on Accept as Solution on the reply which answered your question.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.