cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.9.0 running on macOS 12.3.1 does not allow to download CPU packages. Clicking on the triangle left to the desired CPU family does not open the package selection. Expand all, the packages appear but can not selected for install

MSchm.1
Associate II
 
2 REPLIES 2
Markus GIRDLAND
ST Employee

Hello there,

This is a known issue and a ticket has been written. The current status is that the investigation is still on-going.

Internal Ticket Reference: 119647

I forgot to mention that you can also check out this thread with the same problem where two workarounds are provided:

https://community.st.com/s/question/0D53W00001SeAuQSAV