2024-11-29 01:14 AM
Dear all,
when I press Install button in the Toolchain Manager of the 1.17.0 CubeIDE it hangs after opening the subsequent dialog. I cannot close this dialog with neither mouse nor ESC key, need to terminate the task.
Regards,
Dmitry
2024-11-29 01:22 AM
Hello @DmitryR
Could you provide more information about your OS and environment where you installed CubeIDE?
KR,
Souhaib
2024-11-30 01:59 AM
Hi @Souhaib MAZHOUD ,
Thank you for your attention. My OS is Windows 10 version 22H2 build 19045.5131. System has 16Gb RAM, Typically 40% of it is free when STM32CubeIDE is running. Seems that it stucks on printing a message that is marked red on the image attached.
Regards,
Dmitry