2024-09-18 8:36 AM - edited 2024-09-24 1:16 AM
STM32CubeIDE 1.16.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.12.1 that is available for download.
Main issues fixed in this minor release:
Check the errata under this link for more details.
Where do I obtain STM32CubeIDE 1.16.1?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-27 6:01 AM - edited 2024-10-27 6:02 AM
I was am 1.15.1 and upadte to Ubuntu 24.10.
Suddenly IDE stops at "make" no matter clean or build a project. Could not fix it.
So probably update then.. Update said no updates and an error occurred using the update url that worked before. http://sw-center.st.com/stm32cubeide/updatesite1
Removed and added the update url checked the update url, Ran update. No updates. Went back to update sites. and the just added url was gone ! Done twice, twice auto deleted !
2024-11-04 11:27 AM
Is there a way to change this view back to the older style?
2024-11-06 5:17 AM
2024-11-19 8:13 AM
The instruction at https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Step1_Tools_installation are out of date and don't work exactly with the STM32CubeIDE (version 1.15.1).
It would be really useful to update them:
2024-11-24 11:27 PM
Cyclomatic complexity still doesn't work
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.