cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.13.2 with GCC ARM for STM32 v12.3rel1: nullgcc error

lmartinod
Associate

Hi,

I have STM32CubeIDE v1.13.2 installed and working quite fine.

By default, it is using GCC ARM for STM32 v11.3rel1 (included in the default installation).

I am trying to upgrade the Toolchain with more recent patched STM32 compilers.

I have tried installing both GCC ARM for STM32 v12.3rel1 and GCC ARM for STM32 v13.3rel1 toolchains.

With default v11.3rel1 and newest 13.3rel1, compilation is OK.

But when using v12.3rel1, I encounter the following error: 

"c:/st/stm32cubeide_1.13.2/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.make.win32_2.1.0.202305091550/tools/bin/sh: nullgcc: not found"

 

The toolchains installation seems fine, and I assume I have some issues with environment variables.

When using v11.3rel1 and v13.3rel1 versions, the PATH variable (set to BUILD_SYSTEM by default) includes the "right" directories.

For example, I have (with 13.3rel1):

"C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344\tools\bin;
C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.make.win32_2.1.0.202305091550\tools\bin;"

But when switching to 12.3rel1, the first line is missing by default.

I have tried modifying the PATH variable in order to add this missing path = "C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130\tools\bin;"

Unfortunately, is does not change anything. The compilation error (with nullgcc mention) is still present.

What am I doing wrong here? Have I missed something. Perhaps is it a known issue?

Thank you very much for your help and advice on this topic.

Best regards,

Laurent

 

 

 

4 REPLIES 4

@lmartinod wrote:

I have STM32CubeIDE v1.13.2


That's pretty old.

Why not just update to the latest CubeIDE - currently 1.17.0 ?

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-17-0-released/td-p/747656

 

Of course I would if not other constraints... I am still using Windows 7 and STM32CubeIDE v1.13.2 is the latest version I was able to fully run "smoothly" on Windows 7 PC... With more recent versions, I encounter incompatibilities or issues...

Christian N
ST Employee

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

Try to switch to the "internal builder" , while waiting for more useful replies.

PavelA_0-1734914935749.png