cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.11.0 released

mattias norlander
ST Employee

STM32CubeIDE 1.11.0 was released today on st.com as well as an in-tool update patch.

Caution: The in-tool update does not allow updating debug probe drivers and ST-LINK server tool. Full installer is required for this.

What is new in 1.11.0?

  • Target support updated in-sync with STM32Cube ecosystem in general. In particular:
    • Added the support for one new module in the STM32WL Series
    • Added the support for one new board based on the STM32WB Series
    • Added the support for one board based on the STM32F0 Series
  • New video tutorials added in Information Center
  • SEGGER J-Link update 7.82b
  • Microprocessor Linux® bootloader deployment:
    • Integration of OpenSTLinux Distribution v4.1.0
    • Creation of “MPU SSH weston�? connection for GTK application debug
  • SFRs view update
    • Possibility to create tabs with subsets of peripherals and registers
    • Dump of all peripheral registers to a file
    • Possibility to read the registers via live channel

Additionally a new toolchain based on ST provided GCC-11 will soon be available as an in-tool patch update. 

Known issues fixed and problems and limitations

Please refer to the wiki.

Where do I obtain STM32CubeIDE 1.11.0?

Caution: After updating STM32CubeIDE, the post-update restart fails. STM32CubeIDE must be restarted manually.

0 REPLIES 0