cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE installation issues

tom9900
Visitor

Can multiple versions of a software be installed on one computer or system? The latest version I recently downloaded doesn't include MX. Should I install version 1.19.0, or use the uninstallation method for version 2.0.0?

3 REPLIES 3
Peter BENSCH
ST Employee

Yes, you can install multiple versions of the STM32CubeIDE side by side – in separate directories, of course. On Windows machines, keep the path to them as short as possible, e.g. C:\ST\CIDE2200\.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ozone
Principal III

> The latest version I recently downloaded doesn't include MX.

If it's about that, MX is available as a separate package, it is not integrated in Cube anymore.
There is a thread here about this topic (which I can't find at the moment).

Peter BENSCH
ST Employee

What @Ozone means can be found in the early heads-up and in the announcment, for example.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.