‎2021-12-07 12:37 AM
I upgraded to v1.8 and realized that my programs cannot be downloaded anymore to my discovery STM32L5 board. The error message says:
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 9]
Download in Progress:
Error: Fail to write buffer in flash
Error: failed to erase memory
Upto that message all other status messages looks fine. I assume it is related to ST-LINK GDB server. Version 6.0.0 because in STM32Cube IDE this was version 5.x.x.
The STM32Programmer is still able to download to the board. If I connect the STM32Programmer right after an unsuccessful download of STM32CubeIDE I can see that parts of the memory get deleted but not programmed correct afterwards (see screenshot attached). The first 8 Bytes are correct. After that only erased memory cells are shown.
Would be great if this can be fixed soon.
Best Regards
Markus
‎2021-12-08 6:49 AM
Hello @Community member​ ,
Try to upgrade the ST-Link firmware version, then please tell us if your issue persists.
Imen
‎2021-12-08 8:47 AM
What is the latest ST-Link firmware version?
As the NUCLEO boards were new, STM32CubeIDE imposed to update the ST-Link firmware on first use.
STM32CubeProgrammer and STM32CubeIDE report the version V3J9M3
Now I'm afraid to connect my other boards to STM32CubeIDE because there is a risk of rendering them inoperative...
‎2021-12-08 9:10 AM
Hi Imen,
same as for Nikita. I'm using the firmware version V3J9M3. I actually tried V3J8M3 and had the same issue with STM32CubeIDE 1.8 but not with 1.7
Best Regards
Markus
‎2021-12-09 4:06 AM
Could you try to run ST-Link GDB server in 1.7.0 and in 1.8.0 and activate the gdb server log in your debug configurations and then send the logs to me?
‎2021-12-09 5:01 AM
‎2021-12-12 11:59 PM
I don't see any attached logs. You can either attach them to the forum reply or send them directly in a private message to me!
‎2021-12-13 1:55 AM
‎2022-01-14 6:11 AM
@Markus GIRDLAND​ Any news about the fix of debug bugs of CubeIDE 1.8.0 ?
‎2022-01-19 8:25 AM
got same prob.