2024-03-31 09:58 AM
After updating Cube IDE to version 1.15.0 the memory details & memory regions map in the build analyzer are not showing any informations beside the linker script file name in all my projects start to be bold!!!
Solved! Go to Solution.
2024-04-01 12:31 AM
Hello again @MSale.1
After checking, You have to click on the "Refresh" button:
Refer to the UM2609, section 2.5 where this new button is explained and how you can change the behavior:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-01 12:31 AM
Hello again @MSale.1
After checking, You have to click on the "Refresh" button:
Refer to the UM2609, section 2.5 where this new button is explained and how you can change the behavior:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-28 02:22 PM - edited 2024-06-28 02:27 PM
Thanks! That worked. What about the bold linker script name problem though? Please see the screenshot below.
In the "project explorer" view, The linker script file name is bold (and clipped at the end) for some reason.
EDIT:
It seems like that the project explorer view will slightly clip the end of the longest file name:
2024-09-13 11:45 AM
Ever find an answer to this? I've tried to find the answer in the documentation but was unsuccessful. It's annoying because I can't tell if it's telling me there's a problem or not. There are no errors or warnings from a build., so what's it saying????