2023-10-30 7:21 AM
Hi
I upgrade stmcubeide from 1.12.1 to 1.13.2, after the st-link not work in debugger , i view the followed error:
Failed to bind to port 61235, error code -1: No such file or directory
Failure starting SWV server on TCP port: 61235
Failed to bind to port 61234, error code -1: No such file or directory
Failure starting GDB server: TCP port 61234 not available.
Shutting down...
Exit.
In the previous version the ST-LINK work , what is happend?
I tried with STM32CubeProgrammer to connect to board and programming , work fine.
Solved! Go to Solution.
2023-10-30 7:50 AM
Hello @PZamb.2 ,
First let me thank you for posting.
I suggest that you consult this link: Solved: Re: No ST-Link detected - Only in CubeIDE 1.13.2.
Thanks.
Mahmoud.
2023-10-30 7:50 AM
Hello @PZamb.2 ,
First let me thank you for posting.
I suggest that you consult this link: Solved: Re: No ST-Link detected - Only in CubeIDE 1.13.2.
Thanks.
Mahmoud.
2023-10-30 8:02 AM
Hi thank for your answer, I reboot the pc and now work
2023-11-21 8:26 AM
Hi
now have the same problem again:
Failed to bind to port 61236, error code -1: No such file or directory
Failure starting SWV server on TCP port: 61236
Failed to bind to port 61235, error code -1: No such file or directory
Failure starting GDB server: TCP port 61235 not available.
Shutting down...
I try to replace ST-link server from 2.1.1 to 2.1.o, like suggest from post , but no effect.
The ST-Link works with stm programmer but not work in stm32cubeide 1.13.2 (windows 11).
now reboot of PC don't have effect.
someone have any suggest ?
2024-07-03 1:19 AM
I had exactly same issue with STM32CubeIDE version 1.15.1. Had a NUCLEO-G474RE run over night, then i unplugged to do some work. After replugging the usb cable the debugger no longer worked, and i got the error message:
Failed to bind to port 61236, error code -1: No such file or directory
Failure starting SWV server on TCP port: 61236
Failed to bind to port 61235, error code -1: No such file or directory
Failure starting GDB server: TCP port 61235 not available.
Shutting down...
If i used the STM32CubeProgrammer, then i could connect, program and read the SWD debugging info fine. So the problem must be with the IDE. After some searching around i found a patch that worked for me. The STLink usb driver had to be reinstalled, by running STM32CubeIDE->drivers->STLinkUSBDriver:dpinst_x86.exe(This depends on your CPU). Afterwards the debugger worked again!