cancel
Showing results for 
Search instead for 
Did you mean: 

Sending position information from BissC absolute encoder to STM32F401 via SPI

aknaydn
Associate

Is it possible for BissC absolute encoder to communicate with STM32F401Re via SPI? Or can it be with MAX485 module as in the ardunio example in the link below? 

 

https://protonestiot.medium.com/communication-between-24-bit-rotary-encoder-working-with-biss-ssi-and-arduino-1a85c64b7262

1 REPLY 1
Peter BENSCH
ST Employee

You can take a look at this thread, maybe it will help you?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.