cancel
Showing results for 
Search instead for 
Did you mean: 

run release without breakpoints

Schmid.M.
Senior

Hi,

I flash a project for debugging and set some breakpoints. Then I compile for release and run the code using the green arrow symbol. The code is flashed, but does not run, as it is stuck in a breakpoint from earlier debug sessions.

Is there a way to automatically remove all breakpoints in the device when starting a "Run" configuration?

thanks,

Michael

12 REPLIES 12
Schmid.M.
Senior

I just wanted to have the breakpoints automatically cleared once I start a run session. I thought there were some simple init commands in the run config. Other IDEs do this automatically anyways. Of course I can always disable them manually and then start the run session.

Ok so you've no trouble you're asking for an extra feature so. Go it.

According to me "Run > Skip All Breakpoints" or related toolbar icon usage is not killer here sounds like to me good enough but we may always ask more.

Schmid.M.
Senior

yep. so what are the commands you can enter here? Is there any kind of docu for that? is it GDB commands?

0693W000007BUg2QAG.png