cancel
Showing results for 
Search instead for 
Did you mean: 

[Resolved] STM32CubeIDE project creation issue

Semer CHERNI
ST Employee

Updated post to reflect permanent fix

Dear STM32CubeIDE user,

Further to the recent STM32CubeIDE project creation issue, we would like to inform you that a solution is now available for you.

This permanent fix applies to all STM32CubeIDE versions.

  1. Issue description

When creating a new STM32 project in STM32CubeIDE, the “STM32Cube” radio button may have become unresponsive, blocking the “Next” button after the product selection screen. This prevented the project creation from being completed.

  1. Permanent fix

You can apply this resolution to any STM32CubeIDE version, even if you applied the temporary workaround that we recently shared with you.

  1. Open STM32CubeIDE.
  2. Refresh the database.
    Go to Help > STM32Cube updater > Select “Check the Target selector Device Database Updates”
  3. Restart STM32CubeIDE
  4. If you deactivated the auto refresh function previously, you may wish to reactivate it for all your STM32Cube tools. Here is how to proceed:
  • STM32CubeIDE:
    Go to Window > Preferences > STM32Cube > Firmware Updater.
    Select your preferred auto-refresh option.
  • STM32CubeMX:
    Go to Help > Connection & Updates > Updater Settings.
    Select your preferred auto-refresh option.
  • STMCUFinder:
    Click on the Settings icon > Settings > Updater Settings.
    In the "Database Auto-Refresh" section, select your auto-refresh option.

We apologize for any inconvenience caused by this temporary issue.

If you require further information or assistance, please contact our customer support.

Best regards,

STMicroelectronics

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

43 REPLIES 43
RajvirS
Associate

Thanks for the solution. With Best Regards...

 

fernandolebrato
Associate II

Reinstall the latest version 18.1 from the web portal.
Follow the instructions in 2. Permanent Solution and it's fixed. Thank you.

Tom_pm
Associate III

Refreshing the database in the STM32CubeIDE 1.19.0, and in STM32CubeMX 6.15.0 on Windows 11 I get an error popup about failing to download api_config.json. I never applied the temporary workaround. I guess this is not expected?

See attached picture.

 

 

Hello,

Could you send me the STM32CubeMX.log file found under C:\Users\userID\.stm32cubemx.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks for coming back to me.
In the meantime I could resolve it by applying the stated temporary fix(delete .stm32cubefinder) folder.
And I have also opened a ticket where I have uploaded that folder in the state that cause the problem.
Maybe that helps if you are still doing any further analysis. The ST case number is 00239810.

kentmartin99
Associate

It would be awesome if you would put instructions that matched the ui. Specifically version 1.18 and 1.19 that do not have many of the fields that you have clearly specified for an older version. I am still trying to find where these fields are hidden in the UI. Instrcutions for faulrs should be clear

 

I got the same problem: cube ide is not generating ioc file
project_incomplete.png

it did not enable "next" option, 
grayoption.png

I have latest version 2.0.0 (windows 11)
version2.png

I tried, "Go to Window > Preferences > STM32Cube > Firmware Updater." but that option is not visible, 
not_found.png

also I tried "Go to Help > STM32Cube updater > Select “Check the Target selector Device Database Updates”" but "STM32Cube updater" option is not visible, 
help.png

what can I try now?

Hello @Maurilio-P97 

In the latest release , STM32CubeMX is no more integrated in STM32CubeIDE 2.0.0 

For more details , please check the following LINK

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi there, I have exactly the same problem, and I see your problem is just ignored multiple times, I tried to follow these ignorant answers, but the spaghetti of links followed by further links in endless circle didn't help.. Have you found solution? I also have no 'updater' options in new versions. This update completely set me back by days without warnings!
With kind regards.

Hi
As they mentioned, in the latest release , STM32CubeMX is no longer integrated in STM32CubeIDE 2.0.0 

So now what I do, is first I launch STM32CubeMX and create my project folder
Note: make sure to select STM32CubeIDE, otherwise it won't work (imo it should be selected by default)
example.png

then I open STM32CubeIDE 2.0.0 and import my project folder to start coding.