2024-12-10 02:20 AM - last edited on 2024-12-10 02:25 AM by Andrew Neil
Respected Sir / Madam
I am encountering an issue while debugging an STM32U535 microcontroller using STM32CubeIDE v1.17.0. The details of the environment and error are provided below for your kind reference.
Environment Details
Microcontroller: STM32U535
Debugger: ST-LINK/V2
Software Versions:
STM32CubeIDE: v1.17.0
Operating System: Windows
Error: Data mismatch found at address 0x08010000 (byte = 0x00 instead of 0x08)
Error: Download verification failed
Encountered Error when opening C:\ST\STM32CubeIDE_1.17.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.0.202409170845\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
Final Launch Sequence Error:
Error in final launch sequence:
Failed to execute MI command:
Error message from debugger back end:
Error finishing flash operation
How to fix this issue. Kindly assist me in this regards.
2024-12-12 01:50 AM
Hello @Badrinathan,
First let me thank you for posting and welcome to the ST Community.
For more investigation, I recommend please that you provide your Project File.
Thanks.
Mahmoud
2024-12-12 03:14 AM
Hello @Mahmoud Ben Romdhane
I would like to share the project file for further analysis as suggested. However, I prefer to share it through a private channel instead of publicly.
Could you please let me know the preferred private method to share the file securely?
Thank You
Badrinathan J
2024-12-13 01:06 AM
Hello @Badrinathan ,
I suggest that you share your project through a private message.
Thanks.
Mahmoud
2024-12-23 08:19 PM
Hi @Mahmoud Ben Romdhane
We have shared our project file as you mentioned through your email ID dated 16-12-2024. Kindly assist us in resolving this issue.
Regards
Badrinathan J
2024-12-24 12:53 AM
Hello @Badrinathan ,
I suggest that you upgrade your Debugger ST-LINK to V3 version.
Before programming, I recommend also that you do a full chip erase with STM32CubeProgrammer.
Thanks.
Mahmoud.