cancel
Showing results for 
Search instead for 
Did you mean: 

"Data mismatch" Error while Downloading to STM32U535 using STM32CubeIDE v1.17.0.

Badrinathan
Associate

Respected Sir / Madam

I am encountering an issue while debugging an STM32U535 microcontroller using STM32CubeIDE v1.17.0. The details of the environment and error are provided below for your kind reference.

Environment Details

Microcontroller: STM32U535
Debugger: ST-LINK/V2
Software Versions:
STM32CubeIDE: v1.17.0
Operating System: Windows

Error: Data mismatch found at address  0x08010000 (byte = 0x00 instead of 0x08)  
Error: Download verification failed  

Encountered Error when opening C:\ST\STM32CubeIDE_1.17.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.0.202409170845\tools\bin\STM32_Programmer_CLI.exe  

Error in STM32CubeProgrammer  
Shutting down...  
Exit.

Final Launch Sequence Error:
Error in final launch sequence:  
Failed to execute MI command:  
Error message from debugger back end:  
Error finishing flash operation  

How to fix this issue. Kindly assist me in this regards.

Badrinathan_0-1733825900365.jpeg

 

0 REPLIES 0