cancel
Showing results for 
Search instead for 
Did you mean: 

.project missing from projects created on other computers

SHDK2000
Associate II

Hello,

 

I have previously used a single workspace for developing project in STM32CubeIde on two seperate computers. When I updated to 1.16.0, I can no longer access projects in the workspace when they have been created on the other computer. I get the message:

SHDK2000_0-1723818131600.png

The file is obviously there:

SHDK2000_1-1723818181882.png

 

But I can only open the project on the computer that created the project. This was not a problem when I used version 1.13.0.

 

I use STM32CubeIde revision 1.16.0 running on Windows (10/11) and the workspace is located in a dropbox folder.

 

Any explanation why this doesnt work in newer versions of STM32CubeIde?

 

-S

 

 

 

2 REPLIES 2
SHDK2000
Associate II

Bumb.

Pavel A.
Evangelist III

So the .project file is visible in explorer. Can you open it with a text editor (notepad)?

Can you create a new workspace and import this project, without moving?