2024-03-26 2:20 AM
Hi
Hi
We are using product STM32H56 series , I am encountering problem while building my project
I am using STM32cubeIDE , trust zone enabled .
I enabled X-CUBE-FREERTOS M33non secure
In software package I installed -STm X-CUBE-FREERTOS -CMSIS RTOS2-TZ_non_secure and desired Heap configuartion .
I am getting the error as below .
Please help me to resolve this issue.
Solved! Go to Solution.
2024-03-26 2:39 AM
2024-03-26 2:39 AM
2024-03-26 2:50 AM - edited 2024-03-26 3:08 AM
Thank you for responding back to my post!
I already tried the approach listed in this thread Post ,but I was still facing the issue as listed in the post.
Also I am not able to select the "Copy all used libraries into the project folder"
Can you propose a link/Post where the mention problem is solved .
regards,
Kendall.
2024-03-26 3:27 AM
Thank you for responding back to my post!
I am not able to select the "Copy all used libraries into the project folder" so without selecting I did all the steps suggested in the given Post .I am able to Build the project , But is that the right approach .
Can you please guide me on this.
Thank you.
regards,
kendall