Problem when CubeIDE is installed not in default folder and workspace is also not in default path
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-19 7:38 AM
Hello!
When I install CubeIDE not in default folder and change a folder for workspace there are problems with code generation. This problem occurs with MCUs and Boards. Even if one can generate some code it is not the same code as if the programm and worspace are in default paths. And the debugger does not start...
Labels:
- Labels:
-
STM32CubeIDE
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0