cancel
Showing results for 
Search instead for 
Did you mean: 

post build

Ephraimoved
Associate III

Dear Sir.

I have designed a bootloader that stat from 0x8100000 , length of 40k bytes,

there is also a signature of 2 bytes 0x23,0x45, at @ 0x80f6000,

at last the runtime code that start from 0x8100000.

Is it possible to use STM32IDE's post build to make the bin or hex file 

that will include all 3 sections bootloader, signature, runtime code.

 

 

Please Advise.

 

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

If you can run an executable or batch file, you can do pretty much anything you want.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..