2023-09-22 3:52 AM
Hello team, i have a Nucleo H745ZI_Q board in this am working Differential ADC and Ethernet (using FreeRTOS ) in cortex M7 . ADC is working fine in indivisual code And Ethernet also working fine in indivisual code when going to integrate both in a single code which pheripheral initializing first thats working
1.if i initialize ADC first thats working fine but ethernet is not working
2.if i initialize ehternet first thats working fine but when going to initialize ADC ethernet will not working
am working both ADC and Ethernet in M7 only in ADC not using any RTOS for ethernet using FREE RTOS
What's the issue happening am fail to understand Any help ??
2023-09-22 4:09 AM
Hello @sa V.1
Have you tried without any RTOS ?
Providing more details about the issue would help to investigate further... I suggest using ethernet and ADC examples from CubeH7.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-22 4:23 AM
Ethernet and ADC are independent peripherals and don't directly affect each other. What could be happening is a lack of resources, perhaps you are running too many conversions, or the callback is too slow. Reduce ADC conversion rate by a factor of 100x and try again. If it still doesn't work, provide more detail into what exactly is going on.
2023-09-22 4:47 AM
2023-09-22 5:10 AM
> hadc3.Init.ContinuousConvMode = ENABLE;
> sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
You're swamping the system with interrupts. Increase sample time to max or otherwise decrease the amount of ADC DMA calls that are being produced. Doesn't look like you use the DMA interrupts, so they could be disabled entirely.
2023-09-26 6:00 AM
hadc3.Init.ContinuousConvMode = ENABLE;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
i Checked by increasing and Decreasing SamplingTime But the problem not resolved . Yes sir am not used DMA interrupts is it must to use DMA interrupts ? or i can achive in this method also ...?
// if (HAL_ADC_Init(&hadc3) != HAL_OK)
// {
// Error_Handler();
// }
by commenting this function ethernet will ping .if this function is enabled ADC works but ethernet will not ping i need both should work how can i resolve this sir ??
2023-09-27 12:02 AM
Hello Sir ,Any reply could be very helpfull ...thanks in advance ..