2023-09-02 03:42 AM
Hello STMicroelectronics community,
I am currently working on a project that involves using EEPROM memory with an STM32 microcontroller, specifically [STM32L4R5ZI-P]. microcontroller that does not have internal EEPROM, so I need to use the Flash memory for EEPROM emulation. I've installed the xCube EEPROM package, which provides driver layers and specifies the memory address to use.
However, I'm currently facing an issue with not able write or read from Address[0x080FF000U] , while working with flash that is returning with an error = 160, i will be sharing the snippet for your reference.
HAL_StatusTypeDef HAL_FLASH_Program(uint32_t TypeProgram, uint32_t Address, uint64_t Data)
{
HAL_StatusTypeDef status;
uint32_t prog_bit = 0;
/* Process Locked */
__HAL_LOCK(&pFlash);
/* Check the parameters */
assert_param(IS_FLASH_TYPEPROGRAM(TypeProgram));
/* Wait for last operation to be completed */
status = FLASH_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE);
if(status == HAL_OK)
{
pFlash.ErrorCode = HAL_FLASH_ERROR_NONE;
/* Deactivate the data cache if they are activated to avoid data misbehavior */
if(READ_BIT(FLASH->ACR, FLASH_ACR_DCEN) != 0U)
{
/* Disable data cache */
__HAL_FLASH_DATA_CACHE_DISABLE();
pFlash.CacheToReactivate = FLASH_CACHE_DCACHE_ENABLED;
}
else
{
pFlash.CacheToReactivate = FLASH_CACHE_DISABLED;
}
if(TypeProgram == FLASH_TYPEPROGRAM_DOUBLEWORD)
{
/* Program double-word (64-bit) at a specified address */
FLASH_Program_DoubleWord(Address, Data);
prog_bit = FLASH_CR_PG;
}
else if((TypeProgram == FLASH_TYPEPROGRAM_FAST) || (TypeProgram == FLASH_TYPEPROGRAM_FAST_AND_LAST))
{
/* Fast program a 32 row double-word (64-bit) at a specified address */
FLASH_Program_Fast(Address, (uint32_t)Data);
/* If it is the last row, the bit will be cleared at the end of the operation */
if(TypeProgram == FLASH_TYPEPROGRAM_FAST_AND_LAST)
{
prog_bit = FLASH_CR_FSTPG;
}
}
else
{
/* Nothing to do */
}
/* Wait for last operation to be completed */
status = FLASH_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE);
/* If the program operation is completed, disable the PG or FSTPG Bit */
if (prog_bit != 0U)
{
CLEAR_BIT(FLASH->CR, prog_bit);
}
/* Flush the caches to be sure of the data consistency */
FLASH_FlushCaches();
}
/* Process Unlocked */
__HAL_UNLOCK(&pFlash);
return status;
}
HAL_StatusTypeDef FLASH_WaitForLastOperation(uint32_t Timeout)
{
/* Wait for the FLASH operation to complete by polling on BUSY flag to be reset.
Even if the FLASH operation fails, the BUSY flag will be reset and an error
flag will be set */
uint32_t tickstart = HAL_GetTick();
uint32_t error;
while(__HAL_FLASH_GET_FLAG(FLASH_FLAG_BSY))
{
if(Timeout != HAL_MAX_DELAY)
{
if((HAL_GetTick() - tickstart) >= Timeout)
{
return HAL_TIMEOUT;
}
}
}
error = (FLASH->SR & FLASH_FLAG_SR_ERRORS);
if(error != 0u)
{
/*Save the error code*/
pFlash.ErrorCode |= error;
/* Clear error programming flags */
__HAL_FLASH_CLEAR_FLAG(error);
return HAL_ERROR;
}
/* Check FLASH End of Operation flag */
if (__HAL_FLASH_GET_FLAG(FLASH_FLAG_EOP))
{
/* Clear FLASH End of Operation pending bit */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP);
}
/* If there is an error flag set */
return HAL_OK;
}
here i have provided the function also, where i am facing an error.
could please help me to resolve this issue.
can you please provide any reference to work with microcontroller which we are working.
Thank you.
2023-09-08 11:15 PM
hello,
I have tried this shrink the FLASH but still facing same issue.
this way i have made changes is this correct or need to change, help me to debug this issue.
Thank you,
2023-09-09 02:19 AM
Hello ST Community,
Can anyone suggest a solution for this , I am stuck in this ,atleast if i am doing any mistake while writing open for your suggestion's
Can I get any reference for this microcontroller.
Thanks in Advance,.
2023-09-09 04:32 AM
Documentation on this STM32 says that its flash page size can be 4 or 8 KB depending on some mode.
Are you in the right mode for 4KB page size as you assume?
2023-09-11 04:13 AM
hello,
Yes, I am using 4KB as a size.
Total Flash size is of 2MB,in that for EEPROM Emulation Using 4KB ,as mentioned in datasheet.
Do I need to go through with any other conditions to check?
Thank you.
2023-09-11 04:47 AM - edited 2023-09-11 04:47 AM
Can you find and run some FLASH example for your board first, to verify that erasing a sector and write work correctly?
2023-09-13 03:13 AM
Hello,
when I try to write to Flash I'm returning with an error=160.
Thank you,
2023-09-13 05:28 AM
@yashaswini Does this occur with a simple example (such as some ST Cube FLASH example for a similar board), not the "eeprom emulation"?
2023-09-13 06:20 AM
Yes, for simple example not for an eeprom emulation .
I have attached a snippet of that for reference, in this I'm trying write data to flash in that erasestatus it returns error.
2023-09-13 06:23 AM
2023-09-13 06:28 AM
You're erasing the entire flash in that example. You probably want type FLASH_TYPEERASE_PAGES. You're also sending what looks like an address as the page index.
Perhaps go off of a known working HAL example.