cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple "expected expression before 'do'" errors

SHoll.1
Associate II

I'm new to STM32 and trying to bring up the STM32L053-DISCO project in STM32CubeIDE. It mostly comiles fine, but has an issue with the HAL defines, such as below:

#define __HAL_RCC_GPIOA_CLK_ENABLE()  do { \

                    __IO uint32_t tmpreg; \

                    SET_BIT(RCC->IOPENR, RCC_IOPENR_GPIOAEN);\

                    /* Delay after an RCC peripheral clock enabling */ \

                    tmpreg = READ_BIT(RCC->IOPENR, RCC_IOPENR_GPIOAEN);\

                    UNUSED(tmpreg); \

                   } while(0)

I really don't see why it is being flagged as an error. I'm sure this must have been seen by someone else...

Best regards,

Stephen

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
TDK
Super User

It says *before* do, so before the use of the macro.

If you feel a post has answered your question, please click "Accept as Solution".
SHoll.1
Associate II

One function call upp from this is:

#define __GPIOA_CLK_ENABLE __HAL_RCC_GPIOA_CLK_ENABLE

and before that, this:

#define KEY_BUTTON_GPIO_CLK_ENABLE()      __GPIOA_CLK_ENABLE()

and before that, this:

#define BUTTONx_GPIO_CLK_ENABLE(__INDEX__)   (KEY_BUTTON_GPIO_CLK_ENABLE())

and above that, this:

BUTTONx_GPIO_CLK_ENABLE(Button);

The HAL code is littered with this usage, and it is from a STM sourced project, admittedly written some ago. It must be something obvious but I just don't see what it is.

TDK
Super User

Perhaps you can show the code where the compiler is complaining. The code at and a few lines before __HAL_RCC_GPIOA_CLK_ENABLE is used.

If you feel a post has answered your question, please click "Accept as Solution".
SHoll.1
Associate II

This is where the original function call is from (BUTTONx_GPIO_CLK_ENABLE(Button). It is from the BSP files for the STM32L053-DISCO eval board.

void BSP_PB_Init(Button_TypeDef Button, ButtonMode_TypeDef ButtonMode)

{

 GPIO_InitTypeDef GPIO_InitStruct;

  

 /* Enable the BUTTON Clock */

 BUTTONx_GPIO_CLK_ENABLE(Button);

  

 if (ButtonMode == BUTTON_MODE_GPIO)

 {

  /* Configure Button pin as input */

  GPIO_InitStruct.Pin = BUTTON_PIN[Button];

  GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

  GPIO_InitStruct.Pull = GPIO_PULLDOWN;

  GPIO_InitStruct.Speed = GPIO_SPEED_FAST;

  HAL_GPIO_Init(BUTTON_PORT[Button], &GPIO_InitStruct);

 }

  

 if (ButtonMode == BUTTON_MODE_EXTI)

 {

  /* Configure Button pin as input with External interrupt */

  GPIO_InitStruct.Pin = BUTTON_PIN[Button];

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;

  HAL_GPIO_Init(BUTTON_PORT[Button], &GPIO_InitStruct);

   

  /* Enable and set Button EXTI Interrupt to the lowest priority */

  HAL_NVIC_SetPriority((IRQn_Type)(BUTTON_IRQn[Button]), 3, 0);

  HAL_NVIC_EnableIRQ((IRQn_Type)(BUTTON_IRQn[Button]));

 }

}

TDK
Super User

The problem is

#define BUTTONx_GPIO_CLK_ENABLE(__INDEX__)   (KEY_BUTTON_GPIO_CLK_ENABLE())

When this expands, it puts the code you want to execute within parentheses, which leads to invalid syntax. Just replace that line with the appropriate macro, e.g.

__HAL_RCC_GPIOA_CLK_ENABLE();

If you feel a post has answered your question, please click "Accept as Solution".
SHoll.1
Associate II

So why can't the original code work? It is example code from ST. I would expect the example code to be able to cleanly compile without issue. Is it possibly because a different compiler may have been used? There aren't any compiler dependencies listed in the original code...

TDK
Super User

You're probably using different HAL includes than when the code was written. My guess is that at the time, __HAL_RCC_GPIOA_CLK_ENABLE was written as something that could be evaluated, e.g. REG->CR |= VALUE, instead of its current do/while loop.

You haven't really explained where you got the code, so one can only guess.

Here's one BSP_LED_Init example online that I found which does not use the syntax you're using, and which would compile correctly.

int32_t BSP_LED_Init (Led_TypeDef Led)
{
 GPIO_InitTypeDef gpio_init_structure;
 /* Enable the GPIO_LED Clock */
 switch (Led)
 {
 case LED1:
 LED1_GPIO_CLK_ENABLE ();
 break;
 (…)
 case LEDN:
 LEDN_GPIO_CLK_ENABLE ();
 break;
 default:
 break;
}
 /* configure the GPIO_LED pin */
 gpio_init_structure.Pin = LED_PIN [Led];
 gpio_init_structure.Mode = GPIO_MODE_OUTPUT_PP;
 gpio_init_structure.Pull = GPIO_PULLUP;
 gpio_init_structure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 HAL_GPIO_Init (LED_PORT [Led], &gpio_init_structure);
 
 HAL_GPIO_WritePin (LED_PORT [Led], LED_PIN [Led], GPIO_PIN_RESET);
 return BSP_ERROR_NONE;
}

 Edit: I misread the code. This probably wouldn't compile either.

If you feel a post has answered your question, please click "Accept as Solution".
SHoll.1
Associate II

Thanks for your help.

The code was downloaded from here:

https://www.st.com/en/embedded-software/stsw-stm32152.html

SHoll.1
Associate II

Also, just build the project from STM32CubeMX for the STM32L0538-DISCO and it will try to use the same macros above.