cancel
Showing results for 
Search instead for 
Did you mean: 

Makefile creation

arun27
Associate II

Can you give me a step-by-step guide to create a makefile for stm32 project?

2 REPLIES 2
Ghofrane GSOURI
ST Employee

Hello @arun27 

To generate a Makefile for an STM32 project using CubeMX, follow these steps:

Step 1: Open CubeMX and Configure Your Project

  1. Launch STM32CubeMX 6.13.0 (Link for download  STM32CubeMX - STM32Cube initialization code generator - STMicroelectronics )
  2. Configure your STM32 microcontroller settings, including clock configuration, peripherals, and middleware.

Step 2: Generate the Project

  1. Click on the "Project" tab.
  2. Set the "Toolchain / IDE" to "Makefile".
  3. Specify the project name and location.
  4. Click "Generate Code".

GhofraneGSOURI_1-1736336561681.png

 

   

 

Step 3: Review the Generated Makefile

CubeMX will generate a Makefile in the project directory. This Makefile will include all necessary build rules, compiler flags, and linker scripts based on your CubeMX configuration.

THX

Ghofrane

Is this a continuation of https://community.st.com/t5/stm32cubeide-mcus/compilation-using-batch-file/td-p/759173 ?

If so, perhaps mark the solution there, and give a link to here?

Are you familiar with makefiles in general?